Column Control DTX

Tips for Preventing Damage to Power Sensors and Meters

技術綜覽

Avoid overpowering the power sensor

  • Avoid burning the power sensor by having some idea of the signal level to be measured with the sensor. 
  • Before turning on or turning off the connected equipment or the DUT, reduce the signal level to the minimum safety level. 
  • Properly apply a DC block, limiter or external attenuator as needed. 

Read the warning labels and specifications

  • Do not exceed the values provided in the specifications guide or as indicated by the yellow warning labels on the power sensor and meter.
  • Refer to the specification guide for conditions required to meet the listed specification. 

Protect the RF input connector

  • Be careful not to bend, bump or flex any device under test (DUT) connected to the input of the analyzer (such as filters, attenuators, or large cables). 
  • Ensure externally connected items are properly supported (not freely suspended) from the input.
  • Always use torque wrench and gauge tools for connecting RF connectors.

Follow proper RF cable and connector care

  • Avoid repeated bending of cables. A single sharp bend can damage a cable instantly.
  • Limit the number of connections and disconnections to reduce wear.
  • Inspect the connectors prior to use; look for dirt, nicks, and other signs of damage or wear. A bad connector can ruin the good connector instantly.
  • Clean dirty connectors to prevent poor electrical connections or damage to the connector.

Ensure proper grounding

  • Always use the three-prong AC power cord supplied with the power meter.
  • Proper grounding of the instrument will prevent a build-up of electrostatic charge which may be harmful to the instrument and the operator.
  • Do not damage the earth-grounding protection by using an extension cable, power cable, or autotransformer without a protective ground conductor.
  • Check AC power quality and polarity; typical AC voltage required is 100 V, 120 V, 220 V ± 10% or 240 V +5%/–10%. 

Follow electrostatic discharge precautions

  • Electrostatic discharge (ESD) can damage or destroy electronic components. Whenever possible, conduct testing at a static-safe workstation. Keep electrostatic-generating materials at least one meter away from all components. Before connecting any coaxial cable to instrument, momentarily short the center and outer conductors of the cable together to ground.
  • Always put connector cap on the unused power sensor for preventing ESD.

Check for proper temperature and humidity

  • Keep power sensor and meter in a clean and dry environment. Temperature for typical storage condition is between –40 and 75 °C, humidity < 95 % RH.
  • Ensure proper ventilation among racks. Optimal operating temperature is 23 to –5 °C, always keep instrument ambient temperature at < 30 °C.
  • Cooling vents and fans should be inspected and cleaned frequently

×

請銷售人員與我聯絡。

*Indicates required field

您希望以何種方式取得相關資訊? *必填欄位
Preferred method of communication? 變更email?
Preferred method of communication?

請點擊按鈕後,提供給是德科技您的個人資料。您可以從 Keysight隱私聲明 中,閱讀到我們如何使用這些資料的訊息,謝謝。

感謝您!

A sales representative will contact you soon.

Column Control DTX