Technical Overviews
The Keysight Technologies, Inc. Medalist i3070 light emitting diode (LED) test delivers uncompromising repeatability and accuracy in LED color and luminosity measurements with superior throughput during i3070 in-circuit test. It returns the LED color value and luminosity in nanometers and μW/cm2 to accuracies of ± 3 nm and ± 10% respectively. It can test up to 128 LEDs in less than 1.3 seconds, increasing your i3070 test capacity, which translates to lower cost of in-circuit test.
The i3070 LED test has been designed to enhance the experience of testing LEDs on the i3070. The small sensor design improves the measurement SNR as it can be installed directly over the LED. A shroud tube can be fitted into the sensor to block out ambient light from surrounding LEDs, reducing noise and improving the SNR. If the LED location prevents a direct sensor mount, a light pipe or optical fiber cable can be used to transport the LED light to the sensor.
The sensor can be programmed to return peak (highest), base (lowest) or instantaneous reading of the monochromatic LED’s color and luminosity. For non-monochromatic LEDs, LEDs designed to output multiple wavelengths but perceived by the human eye as a single color, the sensor can be programmed to return a single wavelength with the sensor set to multimode.
LED luminosity can be influenced by temperature and other factors. After turning on the LED, it is desirable to delay the luminosity measurement until it reaches its optimum operation state. The i3070 LED test software gives full flexibility to the test programmer to set the sensor to Trigger, Learn and Evaluate the LED. A Gain is available to increase the LED light input and a Prescaler to set the sensitivity of the sensor. The i3070 LED test sensor has been designed to discern any luminosity changes greater than 3% enabling the i3070 LED Test system to be accurate to within ±10% of the learned luminosity value.
A comprehensive i3070 LED Test experience
The i3070 LED test is integrated with software tools to enhance the programmer experience in developing, debugging and deploying the LED tests on i3070. The software tools will automate the LED test generation and fixture files while a debugging tool aids the programmer to learn and validate the LED test results prior to releasing the tests to manufacturing. The i3070 LED test is supported on i3070 system software release 8.3 or greater.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.