Choose a country or area to see content specific to your location
アプリケーションノート
How Does an Oscilloscope's ADC Impact Vertical Resolution?
All manufacturers specify the number of ADC bits in their oscilloscopes, and resolution is the smallest quantization level determined by the analog-to-digital (A/D) converter in the oscilloscope.
The number of unique digital codes or quantization levels (Q levels) is 2n where n is the number of ADC bits. An 8-bit ADC has 256 Q levels, whereas a 12-bit ADC has 4096 Q levels. Each oscilloscope ADC operates on the oscilloscope’s full scale vertical value. Thus the Q-level steps are associated with the full-scale vertical oscilloscope setting. If the user adjusts the vertical setting to 100 mV per division, for example, full screen equals 800 mV (8 divisions * 100 mV/div) and Q-level resolution is equal to 3.125 mV/level (800 mV divided by 256 levels). If measuring current, for a vertical setting of 10 mA/div, Q-level resolution is set at 312.5 µA/level (80 mA divided by 256 levels)
コンテンツのロックを解除する
無料でお申し込み頂けます
*Indicates required field
ありがとうございました。
フォームが送信されました。
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
営業担当者からご連絡させていただきます。
*Indicates required field
ありがとうございました。
A sales representative will contact you soon.