Column Control DTX

10 Tips to Enhance DC Power Testing and Analysis

Infographics

10 Tips to Enhance DC Power Testing and Analysis

1.      PROGRAM YOUR POWER SUPPLY CORRECTLY TO OPERATE IN CONSTANT 1VOLTAGE OR CONSTANT CURRENT MODE

Constant Voltage: Default operating mode for most power supplies when output is regulating at voltage setting

Constant Current: Power supply switches to CC mode when output is regulating at current limit setting

2.      USE REMOTE SENSE TO REGULATE VOLTAGE AT YOUR LOAD

Output leads can cause a significant voltage drop affecting the voltage across the load.

3.      USE YOUR POWER SUPPLY TO MEASURE DUT CURRENT

A power supply often has enough accuracy to measure a DUTs current eliminating the need for an additional DMM

4.      CONNECT POWER SUPPLY OUTPUTS IN SERIES OR PARALLEL FOR MORE POWER

You can connect two or more power supply outputs in series to get more voltage, or connect outputs in parallel to get more current.

5.      MINIMIZE NOISE FROM YOUR POWER SUPPLY 5 TO YOUR DUT

Start at the Source - Choose a power supply that has low noise

This can be achieved through a typical linear supply or a performance switching supply

SHIELD SUPPLY-TO-DUT CONNECTIONS: The most effective way to remove noise is to ensure your load and sense connections use shielded two-wire cables.

BALANCE OUTPUT-TO-GROUND IMPEDANCE: Use a common-mode choke in series with the output leads and a shunt capacitor from each lead to ground to accomplish this task.

6.      SAFEGUARD YOUR DUT USING BUILT-IN POWER SUPPLY PROTECTION FEATURES

Most DC power supplies have features that protect sensitive DUTs and circuitry from exposure to potentially damaging voltage or current. The most common are:

OVER-VOLTAGE PROTECTION: OVP is a value set in volts designed to protect your DUT from excessive voltage. When the power supply output voltage exceeds your OVP setting, the protection will trip and turn off the output.

OVER-CURRENT PROTECTION: OCP shuts off the output to prevent excessive current flow to the DUT

7.      USE OUTPUT RELAYS TO PHYSICALLY DISCONNECT YOUR DUT

In critical applications where you need to ensure there is no current flowing to or from your DUT you will need to physically disconnect your DUT.

When available, built-in output disconnect relays provide these advantages over external relays

8.      CAPTURE DYNAMIC WAVEFORMS USING A POWER SUPPLY’S BUILT-IN DIGITIZER

When you make a digitizing measurement, you can set two of the following three parameters:

TIME INTERVAL: Time between samples

NUMBER OF SAMPLES: Total number of samples you want to take

ACQUISITION TIME: Total time during which you want to take samples

9.      CREATE TIME-VARYING VOLTAGES USING POWER SUPPLY LIST MODE

The list mode on a power supply can be an effective tool for running two types of tests:

VOLTAGE SEQUENCE TEST: A test where measurements are taken while the DUT is exposed to discrete stimulus voltage values

VOLTAGE WAVEFORM TEST: A test where measurements are taken while the DUT is exposed to a stimulus voltage waveform

10.   CONTROL INSTRUMENTS, AUTOMATE TESTS AND PERFORM ANALYSIS WITH SOFTWARE

CONTROL INSTRUMENTS: Easily connect, record results, and visualize measurements across multiple instruments simultaneously

AUTOMATE TEST SEQUENCES: Rapidly build custom sequences to quickly create tests that used to require days of traditional programming.
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
By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX