Brochures
Scienlab Charging Discovery System
Testing charging function and interoperability
Both development and spread of electric and plug-in hybrid vehicles (EV, PHEV) depend on the expansion and interference-free utilization of the charging infrastructure (electric vehicle supply equipment, EVSE). Due to the relatively recent standards and the resulting lack of experience in the field, faults in the interaction of EV and EVSE can be observed frequently.
Modular Test Environment for Charging Technology
From mobile use to application in the laboratory
The Solution
Keysight Technologies, Inc. offers a modular test environment for EV and EVSE charging systems from mobile use to comprehensive application in the laboratory. The CDS emulates as a central element the charging communication of EV or EVSE. At the same time, the electrical parameters are measured and checked for compliance with standards. The CDS also assumes synchronized triggering of additional power sources and sinks. All components are developed and manufactured by Keysight. Customer-specific requirements or modifications required by the standards can therefore be realized at short notice.
Possible areas of application are:
The following use cases are supported by the CDS:
The Charging Discovery System is designed to be configured in modular arrangements matching the respective application. Its main component is the real-time computer for autonomous execution of test sequences. The test sequence itself is defined and parameterized using the Charging Discover PC software or alternatively controlled directly from a Hardware-in-the-Loop (HiL) system. The CDS provides two manipulable PWM communication interfaces and records, stores, analyzes and evaluates the pilot signals (control pilot/CP, proximity pilot/PP). It also provides digital I/O signals for control and synchronization of external components.
If necessary, this basic configuration can be expanded by additional communication modules for the use of DC charging standards. The following modules can be integrated:
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.