Technical Overviews
Keysight Technologies, Inc. offers a variety of network analyzers with the frequency, performance, and versatility to meet your measurement needs. This selection guide is designed to aid in selecting the required instruments and options to perform calibrated frequency-offset measurements using the PNA and ENA network analyzers.
The PNA and ENA frequency-offset mode options allow the source stimulus and the response receivers to be independently tuned to different frequencies which enable measurements on frequency-translating devices.
Built-in second source
For PNA-X (2- and 4-port) and 4-port PNA-L models, a built-in second source is available to simplify mixer measurement setups eliminating the need for an external LO source, and allowing for LO match, fixed and swept-LO testing. Plus, the internal second source improves sweep speed by at least 20 times compared to using an external source.
Advanced calibrations
The PNA and ENA implement two unique calibration techniques. The scalar-mixer calibration (SMC) is used for high-accuracy, magnitude-only conversion gain/loss measurements and requires a compatible power meter and power sensor. The vector-mixer calibration (VMC) is used for both magnitude and phase conversion gain/loss measurements.
Vector-mixer calibration is optimized for system calibration when phase and absolute group delay measurements are desired. This technique requires a reciprocal calibration mixer. This mixer is specific to each test configuration and must be acquired separately. In addition, the PNA also requires a reference mixer, which need not be reciprocal.
Keysight’s scalar- and vector-mixer calibrations provide you with the tools necessary to determine the characteristics of frequency-translating devices with exceptional accuracy.
PNA Series Network Analyzers
All mixer or converter measurements require Option 080, and most would benefit from either Option 082 or 083. If you want to create and automate custom frequency-offset measurements (for example, intermodulation distortion), you may only need Options 014 and 080. For converters that require input power below –27 dBm, or for devices that have a large amount of LO feedthrough (like an unfiltered mixer), we highly recommend Option UNL, which adds source attenuators. Besides allowing lower input power levels, these attenuators improve the isolation between the PNA’s internal source and LO leakage signals, helping to prevent source-unleveled errors. For devices that put out signals near or above the receiver’s compression levels (which varies between –3 and +5 dBm, depending on the model and frequency), we recommend ordering Option 016, which adds receiver attenuators. Finally, Option 010, which adds time-domain analysis, is very useful for gating out unwanted, time-delayed responses which often occur when measuring mixers.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.