Column Control DTX

KFM and CSAFM/STM for Photovoltaic Characterizations

Application Notes

Photovoltaic (PV) devices are made from various types of semiconductor materials, which are deposited or arranged in a variety of structures. About 90% of the current PV systems are from Si based cells, however, non-silicon based thin-film technologies hold significant growth potential. The three main types of materials used for solar cells are i) silicon, including single-crystalline, multicrystalline, and amorphous Si; ii) polycrystalline thin films, including copper indium diselenide (CIS) and cadmium telluride (CdTe); and iii) single-crystalline thin film of gallium arsenide. There is also research in the areas of organic PV cells and dye-sensitized solar cells (DSC).

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX