Data Sheets
The USB Software Package for Keysight’s InfiniiVision oscilloscopes enables USB 2.0 low-, full-, and hi-speed protocol triggering and decode, as well as USB PD (Power Delivery) trigger and decode. This package also enables other advanced analysis capabilities including USB 2.0 automated signal quality testing, jitter analysis, mask testing, and frequency response analysis (Bode plots) to help test and debug high-speed digital signals, such as USB 2.0.
Introduction
The primary reason engineers use oscilloscopes to debug and characterize serial buses, such as USB 2.0 is because of an oscilloscope’s inherent ability to characterize the analog quality of these signals. Performing analog characterization using an oscilloscope is often referred to as “physical layer” measurements. Table 1 lists the specific measurement capabilities that are enabled on each series with the USB Software Package for Keysight Technologies InfiniiVision X-Series oscilloscopes.
When licensed with the USB Software Package, Keysight’s InfiniiVision 3000T, 4000, and 6000 X-Series oscilloscopes can not only trigger on a broad range of USB 2.0 specific packet types (handshake, token, data, etc.) and errors, but the scope also provides a time-correlated decode trace of each packet below captured waveforms so that you can directly compare the quality of waveforms that produce each decoded byte. In addition, the scope can also display a tabular list of multiple and consecutively captured and decoded packets in the upper half of the scope’s display as shown in Figure 1.
Keysight InfiniiVision X-Series oscilloscopes utilize hardware-based decoding as opposed to conventional oscilloscope software-based decoding. This means that the scope remains responsive and fast when decoding is turned on. And with a virtual real-time update of the USB decode trace, the scope has a much higher probability of detecting infrequent USB errors such as PID errors or CRC errors as compared to other oscilloscopes that utilize software-based decoding.
USB PD (Power Delivery)
Advanced Analysis
USB 2.0 Signal Quality Test
With Keysight’s USB 2.0 signal quality test capability on InfiniiVision 4000 or 6000 X-Series oscilloscopes, engineers now have a more affordable pre-compliance test solution that can perform what many consider to be the most important series of USB 2.0 physical layer tests (signal quality) before running their final product through complete certification testing at a USB-IF designated workshop.
Features:
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.