Data Sheets
Introduction
Complete optical receiver stress test solution for 400GbE optical transceivers with automated stress eye calibration and performance compliance testing.
Optical Receiver Stress Test for 400 Gb/s Ethernet
The telecommunications industry represented by the IEEE decided to address the steadily increasing need for more bandwidth at a lower cost for the intra and inter data centers by combining the spectral efficient PAM-4 modulation with the mature direct modulation/direct detection technology. The shift from NRZ to PAM-4 modulation effectively doubles the line rates, as compared to optical 100 Gigabit ethernet transceivers, while maintaining modulation speed at 26.56125 Gbaud and enabling continued use of some of the existing 100 G components.
Consequently, the compliance test procedures defined for next-generation 400GBASE transceivers are similar to those adopted in IEEE 802.3ba for NRZ-based 100GBASE transceivers. But there are noticeable differences:
Keysight’s N4917BSCB software enables a complete test solution from instrument configuration and
control to automated stressed signal calibration and system performance test, according to IEEE
802.3bs/cd and db specifications (clauses 121, 122, 124, 138, 140 and 167) for following standards:
Automation of the stress signal calibration and conformance tests results in considerable time savings. In addition, the N4917BSCB optical receiver stress test solution provides:
Typical Setup for 200GBASE-LR4/-FR4 Optical Stress Test
The N4917BSCB optical receiver stress test solution consists of a M8040A BERT plus an arbitrary waveform generator for electrical signal and stress generation; an electro-optical converter that modulates the optical signal and a digital sampling oscilloscope which is required for calibration of the stressed eye.
An example setup for 200GBASE-LR4/-FR4 using four 50 Gb/s lanes on four wavelengths in the O-band is shown in Figure 2, which assumes the use of a 200 GAUI- 8 electrical interface. The IEEE 802.3bs standard establishes two ways to provide a clock signal to the digital sampling oscilloscope:
Refer to the configuration guide section for the detailed setup.
Optical Receiver Stressed Test Challenges
The IEEE 802.3 standard describes the optical specifications for optical receivers. The following tables contain the key characteristics 1 of the stress signal measured at TP3 (see Figure 2) to perform stressed receiver sensitivity and jitter tolerance compliance tests. Note that these values are subjected to change in future amendments of the standard. They can be adjusted using the “debug mode” of the Configure tab.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.